Bug in MKL25Z4.h for Initializing UART0 BDH?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Bug in MKL25Z4.h for Initializing UART0 BDH?

跳至解决方案
1,736 次查看
alexdean
Contributor III

I'm looking at the MKL25Z4.H macros for UART0 Baud Rate Generation. The UART0_BDH_SBR(x) macro doesn't seem to take the upper five bits of x, but I believe it should. Is this a bug, am I misusing the macro, or is there a newer version of the file available?

#define UART0_BDH_SBR_MASK  0x1Fu
#define UART0_BDH_SBR_SHIFT 0
#define UART0_BDH_SBR_WIDTH 5
#define UART0_BDH_SBR(x)    (((uint8_t)(((uint8_t)(x))<<UART0_BDH_SBR_SHIFT))&UART0_BDH_SBR_MASK)‍‍‍‍

Here's the version information for the file:

/*
** ###################################################################
**     Processors:          MKL25Z128FM4
**                          MKL25Z128FT4
**                          MKL25Z128LH4
**                          MKL25Z128VLK4
**
**     Compilers:           Keil ARM C/C++ Compiler
**                          Freescale C/C++ for Embedded ARM
**                          GNU C Compiler
**                          GNU C Compiler - CodeSourcery Sourcery G++
**                          IAR ANSI C/C++ Compiler for ARM
**
**     Reference manual:    KL25P80M48SF0RM, Rev.3, Sep 2012
**     Version:             rev. 2.5, 2015-02-19
**     Build:               b150721
**
**     Abstract:
**         CMSIS Peripheral Access Layer for MKL25Z4
**
**     Copyright (c) 1997 - 2015 Freescale Semiconductor, Inc.
**     All rights reserved.
*/‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
标记 (2)
0 项奖励
回复
1 解答
1,487 次查看
mjbcswitzerland
Specialist V

Hi

UART0_BDH has only 5 bits in the divisor and the last three are used for different functions:

pastedImage_1.png

The macro is masking the upper 3 bits (not upper 5) and is therefore OK.

Regards

Mark

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,486 次查看
alexdean
Contributor III

Thanks, now it makes sense. The SHIFT and mask values are from the perspective of each register, rather than the value SBR which spans two registers. So the source code has to extract the upper byte of the desired SBR value before calling the macro.

0 项奖励
回复
1,488 次查看
mjbcswitzerland
Specialist V

Hi

UART0_BDH has only 5 bits in the divisor and the last three are used for different functions:

pastedImage_1.png

The macro is masking the upper 3 bits (not upper 5) and is therefore OK.

Regards

Mark

0 项奖励
回复