Bootloader in MKE04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader in MKE04

647 Views
Afzal1
Contributor I

 

Hi,

We are using bootloader in MKE04Z128VLH4 and we are using Bootloader provided by NXP and it is attached here as well. So the problem we are facing, While updating the HEX file using Kinetis Tool it is showing k_flash_command_failure while uploading the hex files multiple times. If we are uploading same Application HEX file then its get updated otherwise if we try to upload Different Application HEX file using bootloader and Kinetis Tool then it shows the error of command failure.

 

Thanks and Regards

Afzal Hasan

Labels (1)
0 Kudos
Reply
1 Reply

624 Views
FelipeGarcia
NXP Employee
NXP Employee

This is already being discussing in internal ticket. If you have an update, please do not hesitate to let me know.

Best regards,

Felipe

0 Kudos
Reply