Bare metal SD-Card demo for TWR-K60N512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bare metal SD-Card demo for TWR-K60N512

2,097 Views
Thommi_Tulpe
Contributor IV

Hello,

has anyone a  bare metal sd-card demo for the TWR-K60N512 Tower.

 

Thanks

 

0 Kudos
Reply
2 Replies

852 Views
Dekiru
Contributor IV
0 Kudos
Reply

852 Views
mjbcswitzerland
Specialist V

Hi

 

See www.youtube.com/watch?v=AdtRyQ-2IrE (this is for the Kirin3 tower but the Kinetis tower has the same).

 

The demo shown is not 'bare-metal' as such but the SD card module itself is (99%, apart from SD card formating and sector counting as background activity when the info block is lost in FAT32 mode - these can take several minutes / several seconds to complete otherwise on large SD cards).

 

 SD card documentation at http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF (the Coldfire uses SPI and the Kinetis uses either SPI or SDHC interfaces).

 

Regards

 

Mark

 

0 Kudos
Reply