Hi chris gulick ,
After checking the KM34Z256 datasheet and reference manual, it didn't mentioned the GPIO is 5V tolerant pin, so this chip don't have the 5V tolerant.
So,the input voltage should not higher than the VDD.
Wish it helps you!
If you still have questions about it, please kindly let me know.
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------