Any Freedom boards for the new Kinetis V motor control Series?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Any Freedom boards for the new Kinetis V motor control Series?

928 Views
andreag
Contributor II

I didn't see any at the moment, but is anything planned?

As an alternative could you suggest if there is any existing Freedom board I could use as donor by just replacing the MCU? (so basically is there any V series MCU that is pin to pin compatible with another MCU currently used on any Freedom board?

Thanks!

Labels (1)
0 Kudos
4 Replies

706 Views
D_Basler
NXP Employee
NXP Employee

Hi Andrea,

We are currently working to develop a V Series KV1x MCU FRDM board and FRDM Shields for BLDC and PMSM control.

The approximate schedule is Q414.

Rgds

Danny

0 Kudos

706 Views
chris_brown
NXP Employee
NXP Employee

Hi Andrea,

Unfortunately we do not currently have plans to put the Kinetis V series on a Freedom board.  :smileysad:

We do have them on Tower boards though. 

Regards,

Chris

706 Views
andreag
Contributor II

How about the possibility of a FRDM donor board and replacing the MCU with one from the V series with pin to pin compatibility.

Thanks!

0 Kudos

706 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Andrea

No, they are not pin to pin compatibility. So you cannot do in this way. Thanks.

Best Regards

Paul

0 Kudos