About sleep current in STOP mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About sleep current in STOP mode

921 次查看
Sourdev
Contributor II

I am using the S9KEAZN64AMLC microcontroller. I put the device into STOP mode using wfi() instructions. In stop mode, MCU consumes 130uA with a supply voltage of 5V.

In the datasheet, it is mentioned that the stop current is 2uA.

Sourdev_0-1683896618445.png

How I will get 2uA current?

0 项奖励
回复
1 回复

895 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Sourdev,

Do you use the NXP development board to test, or test the circuit board designed by yourself? 

If you are using FRDM-KEAZN32 board, since the convenience of low-power testing is not considered, I am afraid you have to remove several external resistors to get the correct current consumption. You can refer to the discussion in how to achieve the KEA128 lowest static current in STOP mode

If you use circuit board designed by yourself, then please check the external circuit to avoid those case:

Fig3_internalpullupdowncell.JPG


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复