About LOCKUP of MK61FX512VMJ15

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About LOCKUP of MK61FX512VMJ15

1,148 Views
watanabekakeru
Contributor I

Hello,

I have some questions about LOCKUP of MK61FX512VMJ15.

The attahced file is the extract from the reference manual of MK61FX512VMJ15.

The reference manual says that the LOCKUP gives immediate indication of "seriously errant kernel software".

What does "seriously errant kernel software" mean?

When what error in kernel occurs, will LOCKUP occur?

0 Kudos
Reply
1 Reply

1,003 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Kakeru Watanabe,

     The LOCKUP problem is caused by the kernel, just as the RM have described:

This is the result of the core being locked because of an unrecoverable exception following the activation of the processor’s built in system state protection hardware.

    More details about the LOCKUP, you need to check the ARM Cortex M4 core document, I recommend you to refer to this book:

    The definitive guide to ARM cortex M3 and Cortex M4 processors.pdf

   pastedImage_1.png

Wish it helps you!

If you still have question about it, please kindly let me know.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply