About KEAZ128's FMT0 input capture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About KEAZ128's FMT0 input capture

Jump to solution
1,187 Views
shunyizhang
Contributor IV

I'm using keaz128.I want to use ftm0 of keaz128 to capture PWM, calculate the duty cycle and frequency of PWM, is there a corresponding routine to provide.

0 Kudos
Reply
1 Solution
1,155 Views
shunyizhang
Contributor IV
0 Kudos
Reply
2 Replies
1,168 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi shunyizhang,

Please download the FRDM-KEA Quick start package (REV 8 ) from FRDM-KEAZ128: KEA Freedom Evaluation Board.
Please open these examples with S32 Design Studio for Arm 2018.R1 – Windows/Linux(REV 2018-R1) . 
Then you will find FRDM_KEA128_FTM_DualEdge and FRDM_KEA128_PWT examples.

FRDM_KEA128_FTM_DualEdge FRDM_KEA128_PWT.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,156 Views
shunyizhang
Contributor IV

Thanks

0 Kudos
Reply