About KEAZ128's FMT0 input capture

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About KEAZ128's FMT0 input capture

跳至解决方案
1,801 次查看
shunyizhang
Contributor IV

I'm using keaz128.I want to use ftm0 of keaz128 to capture PWM, calculate the duty cycle and frequency of PWM, is there a corresponding routine to provide.

0 项奖励
回复
1 解答
1,769 次查看
shunyizhang
Contributor IV
0 项奖励
回复
2 回复数
1,782 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi shunyizhang,

Please download the FRDM-KEA Quick start package (REV 8 ) from FRDM-KEAZ128: KEA Freedom Evaluation Board.
Please open these examples with S32 Design Studio for Arm 2018.R1 – Windows/Linux(REV 2018-R1) . 
Then you will find FRDM_KEA128_FTM_DualEdge and FRDM_KEA128_PWT examples.

FRDM_KEA128_FTM_DualEdge FRDM_KEA128_PWT.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,770 次查看
shunyizhang
Contributor IV

Thanks

0 项奖励
回复