Ability To Disable EzPort?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Ability To Disable EzPort?

跳至解决方案
1,290 次查看
ee_dugan
Contributor II

Is there a way to disable the EzPort on a MK22FN128VLL10 so that it does not startup during a reset?  Our hardware can hold the EzPort CS high during reset which appears to be enabling the EzPort module?  Is there a way to disable the EzPort during programming with a configuration bit or something?

标记 (2)
0 项奖励
回复
1 解答
1,074 次查看
BlackNight
NXP Employee
NXP Employee

See Disabling EzPort on NXP Kinetis to Solve Power-On Issues | MCU on Eclipse 

There is a bit (at least on K64F) in FOPT to disable EzPort.

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,075 次查看
BlackNight
NXP Employee
NXP Employee

See Disabling EzPort on NXP Kinetis to Solve Power-On Issues | MCU on Eclipse 

There is a bit (at least on K64F) in FOPT to disable EzPort.

I hope this helps,

Erich

0 项奖励
回复