AES and/or DES cryptography for KL16, or KL15 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AES and/or DES cryptography for KL16, or KL15 ?

Jump to solution
1,214 Views
peteklammer
Contributor I

Does Freescale provide or offer C-callable AES and/or DES cryptography functions, optimized for Freescale Kinetis L (Cortex M0) e.g. KL16 or KL15 ?

Labels (1)
0 Kudos
Reply
1 Solution
849 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

If so, the Cryptographic software library is a choice. I do a search and find below cryptographic software library for your reference:

http://www.discretix.com/accelarators/cryptographic-software-librarys/

OpenSSL: The Open Source toolkit for SSL/TLS


Wish it helps.

Best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
849 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Pete,

KL15/KL16 doesn't have hardware cryptographic acceleration unit, which only support software cryptography.

While Freescale doesn't provides related cryptography software so far.

I would recommend customer to use MK11 product, which includes CAU module and Freescale also provide related CAU software lib.

More detailed info, please check below link:

K11_50: Next-Generation Kinetis K11 Baseline 50 MHz MCUs


Wish it helps.

Best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
849 Views
peteklammer
Contributor I


Well, if we could identify an MK11 that was drop-in replacement for KL16, with same pinout, cost, peripherals, and power, that would be a reasonable suggestion.

0 Kudos
Reply
849 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Peter,

MK11 product is better than KL16 product, which also with higher price. MK11 is about 10000 @ US$2.57 each.


Wish it helps.

Best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
849 Views
peteklammer
Contributor I

“Better” is not a single-dimensional scale in this market. If we plan to make 100K of these, then $2.00 apiece BOM throw is $200,000.00 we don’t get to take home. Not to mention battery life, layout real estate, timing and latency differences between Cortex M0 and M4, etc., etc. Better for you is not better for us.

0 Kudos
Reply
850 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

If so, the Cryptographic software library is a choice. I do a search and find below cryptographic software library for your reference:

http://www.discretix.com/accelarators/cryptographic-software-librarys/

OpenSSL: The Open Source toolkit for SSL/TLS


Wish it helps.

Best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply