ADS8332 ADC with K60 Kinetis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADS8332 ADC with K60 Kinetis

1,146 Views
hfabbasi
Contributor III

Can anyody help me in programming ADS8332 using MK60DX256 SDK. Sample code will be highly appreciated.

0 Kudos
Reply
1 Reply

1,140 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

We do not have ADS8332 ADC example, but you can refer the spi examples in SDK_2_2_0_MK60DX256xxx10.

dspi examples.png

Please notice the setting of SPI: 

ads8332 Digital Interface.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply