ADC INTERRUPT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC INTERRUPT

2,995件の閲覧回数
Naveen158
Contributor II

I use KEAZ128AMLH Controller where even though i disable the ADC Interrupt after a particular sequence (and then later enabled again), interrupt is being triggered.

 

Note : AIEN = Low, configured for HW (PIT (TEN, TIE, TIF registers are Low) on interrupt trigger so interrupt should not trigger as AIEN and TEN is low.

ラベル(1)
4 返答(返信)

2,935件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the previous interrupt still valid after you clear AIEN bit.

Pls try to clear the pending bit for the ADC when the clear AIEN bit

NVIC->ICPR[0]|=1<<15;

check if you can enter ISR

BR

XiangJun Rong

0 件の賞賛
返信

2,866件の閲覧回数
Naveen158
Contributor II

No it still hits the ISR even after turning off the PIT and clearing the pending ADC Interrupt

Note :  ADC Interrupt is still enabled

on Disable of ADC, PIT and at the same time clearing its Pending interrupts is solving my issue.

0 件の賞賛
返信

2,967件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that you can use the NVIC module to control the interrupt.

DisableIRQ( ADC0_IRQn);

If you do want to stop ADC conversion, you can set the ADCH as 0x1F.

 

xiangjun_rong_0-1719889359749.png

 

Hope it can help you

BR

Xiangjun Rong

 

0 件の賞賛
返信

2,944件の閲覧回数
Naveen158
Contributor II

Thanks Xiangjun Rong for Answering my Question, the solution you gave me works absolutely fine but it does not solve my root Problem, can you explain me why ISR is executing even though the interrupt is off (AIEN = 0).

0 件の賞賛
返信