32-bit-read burst-inhibited to 16-bit port(no wait states)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

32-bit-read burst-inhibited to 16-bit port(no wait states)

405件の閲覧回数
Taras_Melnik
Contributor I

To Whom It May Concern

Hi, I have a problem very similar to what was expressed in another task: Flex BUS interface issue.( MK66 ) In the linked task, the issue has not been resolved yet. 

I use MK61FX512 controller.

In my case 2 devices connected to 16-bit bus with different CS. AA = 0. Burst modes are disabled.

When I read 16 bit data - all is great. But when I try to read 32 bits through 16-bit bus - only first CSn is asserted, at the same time second TS is asserted correct (fig.1). 

The same behavior is observed on both devices connected to flexbus.

My question is: what may be wrong?

image.png

Figure 1. Diagram observed on slave FPGA.

0 件の賞賛
返信
0 返答(返信)