需要MKE13Z128VLF7的芯片包和例程

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

需要MKE13Z128VLF7的芯片包和例程

Jump to solution
370 Views
abyssnone
Contributor II

MKE13Z128VLF7的芯片包和例程官网上找不到,需要帮忙

 

Tags (1)
0 Kudos
Reply
1 Solution
329 Views
Celeste_Liu
NXP Employee
NXP Employee

IAR不用装pack, device可以直接在线选择:

Celeste_Liu_0-1753956497062.png

 

View solution in original post

0 Kudos
Reply
7 Replies
363 Views
Celeste_Liu
NXP Employee
NXP Employee

您好,MKE13Z128VLF7的SDK在Select Board | MCUXpresso SDK Builder能找到,还可以根据需要自行选择版本或者支持的Toolchain/IDE。

Celeste_Liu_0-1753949682251.png

 

Celeste_Liu_1-1753949716964.png

 

希望上面信息能帮到您。

BRs,

Celeste

 

---------------------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
---------------------------------------------------------------------------------------------------------------------------------

 

 

0 Kudos
Reply
357 Views
abyssnone
Contributor II

方便发送一下链接吗?谢谢

Tags (1)
0 Kudos
Reply
352 Views
Celeste_Liu
NXP Employee
NXP Employee

刚刚发过了:

Select Board | MCUXpresso SDK Builder

打开之后输入“MKE13Z128”就能看到了。

0 Kudos
Reply
342 Views
abyssnone
Contributor II
我下载的keil配置的SDK里面没有找到那个exe文件的PACK安装包
0 Kudos
Reply
340 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello , keil的PACK确实不在我们的SDK中,需要通过KEIL的途径去下载。

我找到了pack的网页链接:Arm Keil | NXP MKE13Z7_DFP

Celeste_Liu_0-1753952838987.png

 

 

或者用pack installer下载也可以:

Celeste_Liu_1-1753952933341.png

 

希望能帮到您。

BRs,
Celeste

0 Kudos
Reply
336 Views
abyssnone
Contributor II
IAR的也是同理吗?谢谢解答
0 Kudos
Reply
330 Views
Celeste_Liu
NXP Employee
NXP Employee

IAR不用装pack, device可以直接在线选择:

Celeste_Liu_0-1753956497062.png

 

0 Kudos
Reply