關於SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

關於SDK

754 Views
JetWen
Contributor I

我嘗試把NXP的SDK 導入IAR的IDE中,但是無法導入,想請問有甚麼我沒有考慮到的因素嗎?

 

0 Kudos
Reply
4 Replies

736 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, as normally when you download the SDK look at the image as an example.

Pavel_Hernandez_0-1699655895272.png

You must select the IDE.

Pavel_Hernandez_1-1699656001831.png

Best regards,
Pavel

0 Kudos
Reply

688 Views
JetWen
Contributor I
Can I import SDK in IAR directly?
or should I create a new project in IAR?
0 Kudos
Reply

677 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, the steps are, download the SDK, unzip the SDK, search for the example that you need to review, on the root C:\Users\mcuxpresso\01\SDKPackages\SDK_2_3_0_EVK-MIMXRT1050\boards\evkmimxrt1050

Then when you open the example on the IAR the IDE automatically will ask you to install the DSP and DFP click yes. 

Best regards,
Pavel

0 Kudos
Reply

662 Views
JetWen
Contributor I

Hello ,I finally got it, thank you for your answer.LOL

0 Kudos
Reply