while flashing i am getting this kind of error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

while flashing i am getting this kind of error

869 Views
remeshck
Contributor I

I am using Kinetis DEsign Studio

while flashing i am getting this kind of error

Open On-Chip Debugger 0.8.0-dev (2015-01-09-16:22)

Licensed under GNU GPL v2

For bug reports, read

  http://openocd.sourceforge.net/doc/doxygen/bugs.html

Info : only one transport option; autoselect 'cmsis-dap'

Error: unable to open CMSIS-DAP device

Error: unable to init CMSIS-DAP driver

Error: Error selecting 'cmsis-dap' as transport

Runtime Error: C:/Freescale/KDS_3.0.0/openocd/bin/..//scripts/kinetis.cfg:3:

in procedure 'script'

at file "embedded:startup.tcl", line 58

in procedure 'interface' called at file "C:/Freescale/KDS_3.0.0/openocd/bin/..//scripts/kinetis.cfg", line 3

Labels (1)
0 Kudos
Reply
1 Reply

741 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Remesh,

Please tell use which board or chip do you use , and which method of flash,

also about your project ,  or the steps about how to reproduce your problem .

Then we can help you .ASAP.

BR

Alice

0 Kudos
Reply