unique SDK path for the KDS 3.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

unique SDK path for the KDS 3.0

跳至解决方案
2,138 次查看
gschelotto
Contributor V

Hello,

I'd like to set an unique SDK path in the project properties. The problem is I share the project with Windows/Linux developers. Under Linux I have to set the path as shown

Screenshot from 2018-01-10 15-54-54.png

while under Windows I have to set the C:/Freescale/KSDK_1.3.0 path.

How can I manage this drawback? I've tried to set a ${variable path} with no success.

regards,

gaston

0 项奖励
回复
1 解答
1,937 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

gaston.

I don't think there is automated conversion option for it.

User needs to modify path setting after porting.

Best Regards,

Jennie Zhang

在原帖中查看解决方案

0 项奖励
回复
7 回复数
1,937 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Gaston.

We can use build variable in SDK path setting, for example:

pastedImage_1.png

Please make sure KSDK_PATH is defined in Build Variables

pastedImage_3.png

I just tested above on my side, the code run normally with these settings.

Please check if this can also work for you.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,937 次查看
gschelotto
Contributor V

Hi Jennie,

The problem is the KSDK_PATH defined in Build Variables is related to the project Properties. If the project of your example above  (with KSDK_PATH set as C:\Freescale\KSDK_1.3.0) is open in a Linux environment it wont work.

An idea is to set the SDK path in Window->Preferences. But where? how?

regards,

gaston

0 项奖励
回复
1,937 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

I don't think window preference can have same feature as you mentioned.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,937 次查看
gschelotto
Contributor V

Hi Jennie,

In this case It wont be possible to open (without path conflicts) the same project on Windows/Linux indistinctly. Could you confirm there is no workaround to solve it?

regards,

gaston

0 项奖励
回复
1,938 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

gaston.

I don't think there is automated conversion option for it.

User needs to modify path setting after porting.

Best Regards,

Jennie Zhang

0 项奖励
回复
1,937 次查看
gschelotto
Contributor V

Jennie, thanks for the update. Yes, in fact this is I'm doing right now. Modifying the path for every OS.

regards,

gatson

0 项奖励
回复
1,937 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

Best Regards,

Jennie.

0 项奖励
回复