Hello,
I'd like to set an unique SDK path in the project properties. The problem is I share the project with Windows/Linux developers. Under Linux I have to set the path as shown
while under Windows I have to set the C:/Freescale/KSDK_1.3.0 path.
How can I manage this drawback? I've tried to set a ${variable path} with no success.
regards,
gaston
已解决! 转到解答。
gaston.
I don't think there is automated conversion option for it.
User needs to modify path setting after porting.
Best Regards,
Jennie Zhang
Hi Gaston.
We can use build variable in SDK path setting, for example:
Please make sure KSDK_PATH is defined in Build Variables
I just tested above on my side, the code run normally with these settings.
Please check if this can also work for you.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jennie,
The problem is the KSDK_PATH defined in Build Variables is related to the project Properties. If the project of your example above (with KSDK_PATH set as C:\Freescale\KSDK_1.3.0) is open in a Linux environment it wont work.
An idea is to set the SDK path in Window->Preferences. But where? how?
regards,
gaston
I don't think window preference can have same feature as you mentioned.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jennie,
In this case It wont be possible to open (without path conflicts) the same project on Windows/Linux indistinctly. Could you confirm there is no workaround to solve it?
regards,
gaston