unable to open CMSIS-DAP device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unable to open CMSIS-DAP device

3,484 Views
gerhardbund
Contributor I

Hello,

during download *.elf file to FRDM-K22F I get following error message:

Info : only one transport option; autoselect 'cmsis-dap'
Error: unable to open CMSIS-DAP device
Error: unable to init CMSIS-DAP driver
Error: Error selecting 'cmsis-dap' as transport
Runtime Error: C:/Freescale/KDS_v3/openocd/bin/..//scripts/kinetis.cfg:3:
in procedure 'script'
at file "embedded:startup.tcl", line 58
in procedure 'interface' called at file "C:/Freescale/KDS_v3/openocd/bin/..//scripts/kinetis.cfg", line 3

Best regards, Gerhard Bund

Labels (1)
0 Kudos
Reply
2 Replies

2,634 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Gerhard

I would recommend updating FRDM-K22F board OpenSDA firmware to J-Link.

Customer could find and download Segger J-Link firmware from:

https://www.segger.com/opensda.html

Please let us know if there still with issues after update with J-Link firmware.

This link should be also helpful:

https://community.nxp.com/docs/DOC-330146

Best Regards
Fiona Kuang
TIC - Technical Information Center

0 Kudos
Reply

2,634 Views
gerhardbund
Contributor I

The problem occurs with Debug_OpenOCD. With Debug_Segger it works.

best regards, Gerhard

0 Kudos
Reply