uart example for FRDM-25z on KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uart example for FRDM-25z on KDS

ソリューションへジャンプ
5,898件の閲覧回数
surenderreddyga
Contributor I

Hi,

 

Can you please provide the code for basic uart application,i.e writing char, reading char.

I tried before, but i was not able to find it

Please help me

ラベル(1)
0 件の賞賛
返信
1 解決策
5,020件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

Attached you can find an example for FRDM-KL25Z using UART1. The examples echoes of the data coming form TX to RX

I hope this information can help you.

Regards,

Adrian

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
5,020件の閲覧回数
surenderreddyga
Contributor I

I am trying to using SDK examples drivers.

UART_HAL_Init(UART1);               //initialize uart

execution is crashing at this point

0 件の賞賛
返信
5,021件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

Attached you can find an example for FRDM-KL25Z using UART1. The examples echoes of the data coming form TX to RX

I hope this information can help you.

Regards,

Adrian

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,973件の閲覧回数
anuj_msee
Contributor I

I am using mcuexpresso in my macbook to perform uart code for the frdmkl25z to read the input from GPIO bus, but the code you send in the .rar is not working as the only library I am having is "incude<MKL25Z4.h". Also if you can guide me on servo coding for self driving steering control and dc speed control i will be very thankful to you.

0 件の賞賛
返信
5,020件の閲覧回数
surenderreddyga
Contributor I

Hi

That is working fine with the hardware also. Now have to analyze my code why it is crashing.

Thanks for the support..................................................

0 件の賞賛
返信
4,971件の閲覧回数
anuj_msee
Contributor I

Looks like library error. My MCUEXPRESSO IDE when i selected board package i only have option for the "include<MKL25Z4.h".

0 件の賞賛
返信