tip: printing codesize to console

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tip: printing codesize to console

2,792件の閲覧回数
macl
Senior Contributor I

Hi,

Just posting a tip that I found.  If you are like me and hate combing through a map file just for a quick look at a project's codesize, then luckily there is a nice utility built into Kinetis Design Studio from the GCC Toolchain.  I noticed that the switch to turn this on is in a different place than it was in CodeWarrior.

 

Go to Project…Properties…C/C++ Build…Settings…

 

On the Toolchains tab check Print size

 

15486_15486.pngprintsize.PNG.png

 

Now you will see code size information in the Console window when you build the entire project.

15487_15487.pngkds_print_size_example.PNG.png

Mac

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 返信

1,687件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Mac,

thanks for sharing your tip!

Links related to that topic:

Erich

0 件の賞賛
返信