"Install New Software" bug in KDS3?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

"Install New Software" bug in KDS3?

963 次查看
michaelhuslig
Contributor IV

When I click Help|Install new software and select an available software site such as the Freescale KDS Update Site, I see several updates that are already installed, even though the "Hide items that are already installed" box is checked.

标签 (1)
0 项奖励
回复
3 回复数

800 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Michael,

On my side ,  it without error . Please screenshot yours .

pastedImage_0.png

BR

Alice

0 项奖励
回复

800 次查看
michaelhuslig
Contributor IV

Hello Alice,

I was seeing the unexpanded 4 entries (KDSK 1.2.0 Eclipse Update, etc).  I could select and deselect each and all.  I didn't think to expand the entries;  I would have seen then there were no updates that hadn't been installed already.  But I would have expected that no entries would have been shown at all if the "Hide items already installed" was checked.

Mike

0 项奖励
回复

800 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mike,

After select "Hide item...." , all the items which  are shown on the window is have not been updated.

After you updated them , it will not show.

For example , i update the "KSDK1.2.0 Eclipse Upddate" , after update, it will as this :

pastedImage_0.png

Maybe you think you have instll KSDK1.2, while this is update it .


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复