programming connections for MKE04 series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

programming connections for MKE04 series

2,303件の閲覧回数
jamespottebaum
Contributor I

how to you provide for programming of the MKE04 series of micros

can not find any documentation anywhere - - -

 

what combination of pins needs to be brought out.

 

also what interface module is needed to program the PCB from a PC

 

Jim P

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

1,683件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi James,

we can use Multilink Universal or  Multilink Universial FX to program KE04

P&E Microcomputer Systems - USB Multilink Universal - USB Multilink Universal All-In-One Development...

P&E Microcomputer Systems - USB Multilink Universal FX - USB Multilink Universal FX All-In-One Devel...

we can refer FRDM-KE04Z schematic SWD design for how to design program interface.

http://cache.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KE04Z_SCH.pdf

if you already purchased FRDM-KE04Z board, you can debug and program KE04z via OPENSDA usb interface, needn't external programmer.

Freescale Freedom Development Platform for th|Freescale

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,683件の閲覧回数
jamespottebaum
Contributor I

that helps.

looking at the FRDM-KE04Z, do I have to add the 10 pin micro connector?

Jim P

0 件の賞賛
返信

1,683件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi James,

The FRDM-KE04Z Freedom boards have on-board debugger capability via the USB connector.  You do not need to populate the 10-pin header.  The USB provides power, debugging, Virtual COM Port, and debugger firmware update capabilities.

For a custom product you develop, then you would need to have a 10-pin debugger header that will work with PEMicro, Segger, and other debugger hardware.

Regards,

David

0 件の賞賛
返信

1,683件の閲覧回数
jamespottebaum
Contributor I

I am developing my own board and need to program it - - - -

from the pictures, the 10 pin programming connector is not installed on

the FRDM - - - -

can I install it and use it to program my own MKE04 design

Jim P

0 件の賞賛
返信

1,683件の閲覧回数
DavidS
NXP Employee
NXP Employee

Seems like it would work.

Please review this great blog (and signup for it too).

Using the Freedom Board as SWD Programmer | MCU on Eclipse

Regards,

David

0 件の賞賛
返信