mqxlite problem starting template tasks that were not marked as MQX_AUTO_START_TASK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mqxlite problem starting template tasks that were not marked as MQX_AUTO_START_TASK

1,986 次查看
markschuck
Contributor II

Hi,

 

I've been testing/using the mqxlite component in KDS with processor expert.

 

I've added 3 tasks to the template list, the first task is my startup task and the other two tasks implement product specific functions using some other processor expert LDD's. They are not marked auto start (TASK_ATTRIBUTES does not have MQX_AUTO_START_TASK set).

 

The start up task creates some events/timers/semaphores for synchronization and then the intention is to have it start the other tasks.  However i can't seem to find an MQX Lite function to start tasks that were included in the task template list.

 

_task_create(...) looks like it is what i want but:

1) it is not defined in any include file.

2) it does not work correctly because it eventually calls _task_build_internal with stack_ptr and stack_size set to null/0. This causes that function to try and allocate them again even though processor expert already globally allocated stacks with the size that i selected in the UI.

3) calling it anyways eventually results in an unhanded interrupt and a (debug) halt.

 

Maybe there is a function that already exists but i could not find it.

I dont' have any experience with MQX lite and the older code warrior so i have no idea if this is specific to KDS or not....

 

For now, I've hacked up my own task_create_from_template function that traverses the task template list and it works just fine, code is bellow.

 

void task_create_from_template(uint32_t taskNumber)

{

    _int_disable();

 

    extern KERNEL_DATA_STRUCT_PTR _mqx_kernel_data;

    extern TD_STRUCT_PTR _task_init_internal(

        TASK_TEMPLATE_STRUCT_PTR template_ptr,

        _task_id                 creator_task_id,

        uint_32                  create_parameter,

        boolean                  dynamic,

        pointer                  input_stack_ptr,

        _mem_size                input_stack_size

    );

 

     //GER_KERNEL_DATA macros is defined in some internal MQX lite header

     //I'd rather not include that in this file, so the implementation was in-lined manually

    KERNEL_DATA_STRUCT_PTR kernel_data = _mqx_kernel_data;

    {

        TD_STRUCT_PTR               td_ptr;

        TASK_TEMPLATE_STRUCT_PTR    template_ptr;

        int                         task_index = 0;

 

        template_ptr = kernel_data->INIT.TASK_TEMPLATE_LIST;

 

        while (template_ptr->TASK_TEMPLATE_INDEX) {

            if (template_ptr->TASK_TEMPLATE_INDEX == taskNumber) {

                td_ptr = _task_init_internal(template_ptr,

                                             kernel_data->ACTIVE_PTR->TASK_ID,

                                             template_ptr->CREATION_PARAMETER,

                                             FALSE,

                                             (pointer)mqx_task_stack_pointers[task_index],

                                             (_mem_size)template_ptr->TASK_STACKSIZE);

 

                _task_ready_internal(td_ptr);

 

                _int_enable();

                return;

            } /* Endif */

            ++template_ptr;

            ++task_index;

        } /* Endwhile */

    }

 

    _int_enable();

}

标签 (1)
标记 (4)
0 项奖励
回复
1 回复

1,578 次查看
davidsherman
Senior Contributor I

Did you try using _task_create_at() to start the non-auto tasks?  I have been using this to start MQX Lite taks that did not have the AUTO_START enabled.

0 项奖励
回复