When I used S32DS to start my design, first i established a s32ds application project, the debugger tool which i chioced was segger J-Linker GDB server, after the project completed, it was build seccesfully, when i debuggered this project, it jumped to DefaultISR: ldr r0, =DefaultISR, the code showed below:
#include "derivative.h" /* include peripheral declarations SSKEAZ64M4 */
#include "gpio.h"
int main(void)
{
CONFIG_PIN_AS_GPIO (GPIOB, PTG0, 1); // TLE7240_RST1_P48 Low active
OUTPUT_SET(GPIOB, PTG0);
#define COUNTER_LIMIT 100000
int counter = 0;
for(;;) {
counter++;
if(counter > COUNTER_LIMIT) {
counter = 0;
OUTPUT_TOGGLE(GPIOB, PTG0);
}
}
return 0;
}
but when i choiced PE Micro GDB server, the same project had no such problem, what's the reason? thanks for replay.
Hello ,
Please share your whole project ,I will test it on my side .
If it is a private one , you can also submit a service request to attach it :
BR
Alice