ke06z64 chip can not be downloaded KE06Z64芯片出现下载不了的问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ke06z64 chip can not be downloaded KE06Z64芯片出现下载不了的问题

1,233 Views
harry200899
Contributor I

求助:KE06Z64芯片出现下载不了的问题:

Help: ke06z64 chip can not be downloaded

Keil5通过J-Link将程序下载至电路板的KE06Z64芯片(4M外部晶振),弹出窗口提示Error:Flash Download failed - "Cortex-M0+"。

Keil5 downloads the program to ke06z64 chip (4m external crystal oscillator) of the circuit board through j-link, and a pop-up window prompts error: Flash download failed - "Cortex-M0 +".

我的界面设置如下:

My interface settings are as follows:

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

pastedImage_5.png

pastedImage_6.png

pastedImage_7.png

pastedImage_8.png

pastedImage_9.png

pastedImage_10.png

pastedImage_11.png

pastedImage_12.png

pastedImage_13.png

Labels (1)
0 Kudos
4 Replies

1,082 Views
harry200899
Contributor I

The problem has been solved:Setting of "ram for algorithm"。

pastedImage_1.png

0 Kudos

1,082 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi jiangen,

Jlink can read out IDCODE, the physical connection if fine. KE06 has SDK. Please download KE06 SDK from Welcome | MCUXpresso SDK Builder 

There are lots of Keil example project in it. Please try these project.

Jlink has a software and tool pack. You can download from https://www.segger.com/downloads/jlink/JLink_Windows.exe 

Use J-link commander, type "connect" to test connection.

If it shows the device is locked, type "unlock kinetis"

Regards,

Jing

0 Kudos

1,082 Views
harry200899
Contributor I

Who can help me solve this problem? Thank you!

0 Kudos

1,082 Views
harry200899
Contributor I

Who can help me solve this problem? Thank you!

0 Kudos