j-link GDB Server failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

j-link GDB Server failed

2,393 Views
dharmeshkanzari
Contributor II

Hello,

 

i am using FRDM k82f board. And my ide is KDS 3.2. But whaen i am trying to load some code in my board i face error "j-link GDB Sereve failed". Please see attached file.

Onr more thing i am using "opensda v2.1.bin" file in my board for jlink drivers.

 

Please help me to solve this problem

 

Thanx,

Dharmesh

Original Attachment has been moved to: OpenSDA_V2_1-(1).bin.zip

Labels (1)
0 Kudos
Reply
3 Replies

1,975 Views
harshpatel
Contributor IV

Hello Dharmesh

This error may occurs due to improper j link to Controller connection. Make sure that jlink pins 1,3,2,4 and 10 is connected to relevant controller SWD pins. Jlink pin outs are as follows:

jlink_pin_outs.png

Let me know if any....

Thanks & regards

Harsh

0 Kudos
Reply

1,975 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Harsh,

If you  use the demo board frdm-k82 , and the jink debugger ,

please first make the connect is right , then check the configuration of KDS debug view .

Hope it helps

Alice

0 Kudos
Reply

1,975 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Dharmesh,

Please show the debugger configuration view on your side .

And also you'd better show the steps one by one how do you download project .

What about your PC system ?

I used Windows , it can work well .

BR

Alice

0 Kudos
Reply