how to flash/debug using KL05Z+JLINK+KDS 2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to flash/debug using KL05Z+JLINK+KDS 2.0

ソリューションへジャンプ
2,062件の閲覧回数
gschelotto
Contributor V

Hello,

 

I'd like to flash/debug a KL05Z device using 5 pin (GND, 3V3, DIO, CLK, RST) with J-LINK Base and Kinetis Design Studio v2.0. Could anybody help me?

 

Thanks in advance,

gaston

ラベル(1)
タグ(1)
1 解決策
1,674件の閲覧回数
BlackNight
NXP Employee
NXP Employee
5 返答(返信)
1,674件の閲覧回数
santiago_gonzal
NXP Employee
NXP Employee

Hello Gaston,

What is your issue?

- How to do the hardware connection of the pins?

- How to create the debug configuration in KDS?

- How to create a project to flash inside the KL05 using KDS?

Regards,

Santiago

0 件の賞賛
返信
1,674件の閲覧回数
gschelotto
Contributor V

Hello Santiago,

Sorry for not being so clear.

Here's my current HW configuration

Untitled.png

So the question is related to how to create the debug configuration in KDS 2.0 with J-LINK.

regards,

gaston

0 件の賞賛
返信
1,675件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi gaston,

have a read here: https://community.freescale.com/docs/DOC-101845

Erich

1,674件の閲覧回数
gschelotto
Contributor V

Hi Erich,

I've followed the steps for the Segger J-LINK configuration but I get the next error

Untitled.png

I've also checked the trouble shooting tips but I'm still not able to start a debug session. Any hints?

regards,

gaston

0 件の賞賛
返信
1,674件の閲覧回数
gschelotto
Contributor V

Solved! I forgot to set GDB executable path correctly.

regards,

gaston

0 件の賞賛
返信