Hi,
I'd like to write some MQX application code in KDS 1.1.1. But I am having trouble creating a new MQX project in KDS. In CodeWarrior, I can create a MQX by File->New->MQX 4.1 Project, but I didn't find this option in KDS. What I am doing now is to import sample MQX projects and modify the project, which I find very inconvenient. Is there a way to create MQX project in KDS? Please advise.
Thank you!
Tuo
解決済! 解決策の投稿を見る。
Hello Tuo and Arthur ,
Official support of KDS in MQX is planned in MQX 4.2 & MQX 5.0 coming later this year.
At that time MQX plug-ins for KDS (e.g. Task Aware Debug & New Project Wizard) will be available. Also, MQX project files for all libraries and examples will be available for KDS.
And now ,
Create MQX project on KDS , you can refer to :
4. first, search ''MQX_ROOT_DIR'' , and change the only first one, change <stringMacro name="MQX_ROOT_DIR" value="${ProjDirPath}/../../../../../.."> to <stringMacro name="MQX_ROOT_DIR" value="C:\Freescale\Freescale_MQX_4_1"> ;
second, search ${ProjDirPath}/../../../../../.. and change all of to ${MQX_ROOT_DIR}
5.Save the changes
6. Import the project into KDS and build. You should build without errors.
7.Change the project name if you want and now you have a MQX Template project that you can copy&paste any times and add the new sources.
Best Regards,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you for your support to us!
So I created a mqx project on KDS and added all libraries, when i built it. It thew me an error:
Description | Resource | Path | Location | Type |
make: *** No rule to make target `C:/Freescale/KSDK_1.1.0/lib/ksdk_mqx_lib/kds/K60D10/Debug/libksdk_platform_mqx.a', needed by `mqx_tutorial.elf'. Stop. | mqx_tutorial | C/C++ Problem |
I checked the folder and it doesnt contain the file. Does anybody know what happened?
Hi Yaran,
Do you want to use the mqx of KSDK ?
If yes, you need build the two lib :
and if you want to create KSDK-PE project , directly create KSDK project , then add the MQX component .
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Piotr,
Thanks for sharing!
Tuo
Hello Tuo and Arthur ,
Official support of KDS in MQX is planned in MQX 4.2 & MQX 5.0 coming later this year.
At that time MQX plug-ins for KDS (e.g. Task Aware Debug & New Project Wizard) will be available. Also, MQX project files for all libraries and examples will be available for KDS.
And now ,
Create MQX project on KDS , you can refer to :
4. first, search ''MQX_ROOT_DIR'' , and change the only first one, change <stringMacro name="MQX_ROOT_DIR" value="${ProjDirPath}/../../../../../.."> to <stringMacro name="MQX_ROOT_DIR" value="C:\Freescale\Freescale_MQX_4_1"> ;
second, search ${ProjDirPath}/../../../../../.. and change all of to ${MQX_ROOT_DIR}
5.Save the changes
6. Import the project into KDS and build. You should build without errors.
7.Change the project name if you want and now you have a MQX Template project that you can copy&paste any times and add the new sources.
Best Regards,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you for your support to us!
Hi Alice,
Thank you very much! I followed your instructions and I can build this new project without any problems. One comment I have is that the "Source" folder in the hello sample project is a virtual folder so I need to create a "real" folder and add source files into it.
Thanks again!
Regards,
Tuo
Hi,
I have the same problem.
Are they a simple way to create It?