Hello,
i'm using a kl46 with kds 3.1 and the sdk 1.3. I have a problem with this function where i change the frequency of my cpu according with some flag:
void CPU_Clock_Setting(void) {   int i = 0;   byte error = 0;     DisableInterrupts;   if (flag_lcd || flag_usb) {//se LCD on o USB inserita vado alla max freq   error = CLOCK_SYS_UpdateConfiguration(0, kClockManagerPolicyForcible);   i = CLOCK_SYS_GetCoreClockFreq(); #ifdef DEBUG   LPSCI_HAL_SetBaudRate(UART0_BASE_PTR, i, 115200); #endif   I2C0_SetClockConfiguration();   ADC_SetClockConfiguration();   } else{//altrimenti scendo alla configurazione di risparmio   error = CLOCK_SYS_UpdateConfiguration(1, kClockManagerPolicyForcible);   i = CLOCK_SYS_GetCoreClockFreq(); #ifdef DEBUG   LPSCI_HAL_SetBaudRate(UART0_BASE_PTR, i, 115200); #endif   I2C0_SetClockConfiguration();   ADC_SetClockConfiguration();   }   EnableInterrupts; }
the problem is when the function CLOCK_SYS_UpdateConfiguration is called, when the fsl_debug enter in the function
void LPSCI_HAL_SendDataPolling(UART0_Type * base,                                const uint8_t *txBuff,                                uint32_t txSize) {     while (txSize--)     {         while (!UART0_BRD_S1_TDRE(base))         {}           LPSCI_HAL_Putchar(base, *txBuff++);     } }
it remain in the while loop. why this? i have add the function LPSCI_HAL_SetBaudRate for re-set the clock of the UART but same problem. Thanks
Configur
Hello Alice,
yes but my problem is to pass from PLL to BLPE mode. In this mode the UART crash and there is no reason. Now i'm bored to try to find a solution (if there is....), i will use the PLL in all two configuration. The micro will consume more power ....
Thanks
Hello Daniele,
The clock source of the UART0 not the CPU core clock , so there is some error :
And about configure the clock and the baud rate , i recommend you refer to the demo code under KSDK1.3:
\KSDK_1.3.0\examples\frdmkl46z\driver_examples\lpsci\lpsci_blocking\kds
in the initialize function , you can hwo to configure the clock source of UART and the baud rate :
// Initialize the lpsci module with base address and config structure
LPSCI_DRV_Init(BOARD_DEBUG_UART_INSTANCE, &lpsciState, &lpsciConfig);
Hope it helps
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
i have tried to set the clock source of the lpsci to ESC source (i have a 16mhz oscillator)
when i call the function :
void CPU_Clock_Setting(void) {
int i = 0;
byte error = 0;
DisableInterrupts;
if (flag_lcd || flag_usb) {//se LCD on o USB inserita vado alla max freq
error = CLOCK_SYS_UpdateConfiguration(0, kClockManagerPolicyAgreement);
//CLOCK_SYS_SetConfiguration(&clockMan1_InitConfig0);
i = CLOCK_SYS_GetCoreClockFreq();
#ifdef DEBUG
//CLOCK_SYS_SetLpsciSrc(0, kClockLpsciSrcOsc0erClk);
//LPSCI_HAL_SetBaudRate(0, i, 115200);
//i = CLOCK_SYS_GetLpsciFreq(0);
#endif
I2C0_SetClockConfiguration();
ADC_SetClockConfiguration();
} else{//altrimenti scendo alla configurazione di risparmio
error = CLOCK_SYS_UpdateConfiguration(1, kClockManagerPolicyAgreement);
//CLOCK_SYS_SetConfiguration(&clockMan1_InitConfig0);
i = CLOCK_SYS_GetCoreClockFreq();
I2C0_SetClockConfiguration();
ADC_SetClockConfiguration();
}
EnableInterrupts;
}
all work fine but after the exit from this function LPSCI_HAL_SendDataPolling is called and the TDRE flag is set to 0 and the code stop in the while loop:
void LPSCI_HAL_SendDataPolling(UART0_Type * base,
const uint8_t *txBuff,
uint32_t txSize)
{
while (txSize--)
{
while (!UART0_BRD_S1_TDRE(base))
{}
LPSCI_HAL_Putchar(base, *txBuff++);
}
}
the problem is that i can't see the function that has tried to send data because i have this condition:
 
it is possible increase the number of function so i can reconstruct the function that call this?
Hello Daniele,
- After run here
how about continue to run ?
- " it is possible increase the number of function so i can reconstruct the function that call this? "
Do you meaning you want change the function of "LPSCI_HAL_SendDataPolling", yes , you can .
BR
Alice
Hello,
i have tried some solution in this days but nothing works.
I have define a static callback in the fsl_clock_manager
that do this (i have follow this
https://app-community.freescale.com/docs/DOC-329554):
clock_manager_error_code_t clockMan_uart0_callback(clock_notify_struct_t
notify, void * callbackData)
{
clock_manager_error_code_t result = kClockManagerSuccess;
switch (notify->notifyType) {
case kClockManagerNotifyBefore:
DbgConsole_DeInit();
break;
case kClockManagerNotifyRecover:
break;
case kClockManagerNotifyAfter:
CLOCK_SYS_SetLpsciSrc(0, kClockLpsciSrcOsc0erClk);
DbgConsole_Init(0, 115200, kDebugConsoleLPSCI);
break;
default:
result = kClockManagerError;
break;
}
/* Write user code here */
return result;
}
the clock surce of the uart0 is always the oscerclk
but the firmware continue to lock at the function
with the register setting as is
PS: i'm using FREERTOS
Il 23/02/2016 04:12, Alice_Yang ha scritto:
>
NXP Community
<https://community.freescale.com/?et=watches.email.thread>
>
fsl_debug problem change frequency
risposta da Alice_Yang
<https://community.freescale.com/people/Alice_Yang?et=watches.email.thread>
su /Kinetis Design Studio/ - Visualizza la discussione completa
<https://community.freescale.com/message/617635?et=watches.email.thread#617635>
>
Hello Daniele,
From your screenshot, i see the TDRE bit has set to 1, so i think it can jump to the loop
      while (!UART0_BRD_S1_TDRE(base))  
Could you please test the demo code under KSDK1.3 on your board :
KSDK_1.3.0\examples\frdmkl46z\driver_examples\lpsci\lpsci_polling\kds 
Alice
Ok, solved the problem with the timer using the function
CLOCK_SYS_SetPllfllSel(kClockPllFllSelPll); but with the fsl_debug the
problem stay on.
Il 02/03/2016 10:30, Alice_Yang ha scritto:
>
NXP Community
<https://community.freescale.com/?et=watches.email.thread>
>
fsl_debug problem change frequency
risposta da Alice_Yang
<https://community.freescale.com/people/Alice_Yang?et=watches.email.thread>
su /Kinetis Design Studio/ - Visualizza la discussione completa
<https://community.freescale.com/message/620493?et=watches.email.thread#620493>
>
Hello Daniele,
After you change the clock of cpu, you need refer to the initialize code to configure the clock of UART,
and i have not see you re-configure the UART clock , and i don't know the "fsl_debug problem" detail,
so you can send your project to me , i can debug it , then check the problem .
BR
Alice
Hi,
any news?
--
*OPTOI GROUP *
Technical Dept.
Daniele Cortellazzi
***************************************************
OPTOELETTRONICA ITALIA S.r.l.
Via Vienna, 8
I-38121 Gardolo (TN) ITALY
Phone 0039 0461 991121
Fax 0039 0461 990164
daniele.cortellazzi@optoi.com
Hello Danniele,
I had intended to change the project correct then send o you , but
the project on my side sometimes can not run into the "main_task()",
for i know little about the RTOS, so i can only check the code without debug.
First , in the function of
the callback function will initialize the peripherals clock, for example the UART, and this needs to be
implemented manually , while in your project , it is null , so it have not update the uart clock .
And about the change clock configuration, i highly recommend you one demo , it use KSDK1.2 , while
the method is the same , you can refer to : https://community.freescale.com/thread/357115#524685
Hope it helps
Alice
Hello,
i have just tried with the use of the callback function but same
problem. I have change some part in the code:
- remove the WAIT component in pex because i not use it
- i use the callback function for deinit e init the UART
(clockMan_uart0_callback)
to do the same things in the sample, the device still to not work.
In my project i use a 16mhz crystal but the frdm mount a 8mhz,
could be this to give you problem?
The firmware is very simple, it print "HELLO" and when the pin PTD6 is
pulled down the interrupt PORTC_PORTD_IRQHandler is called, the
CPU_Clock_Setting() function is executed and a change in frequency is
required.
Thanks
*
Il 16/03/2016 05:25, Alice_Yang ha scritto:
>
NXP Community
<https://community.freescale.com/?et=watches.email.thread>
>
fsl_debug problem change frequency
risposta da Alice_Yang
<https://community.freescale.com/people/Alice_Yang?et=watches.email.thread>
su /Kinetis Design Studio/ - Visualizza la discussione completa
<https://community.freescale.com/message/625200?et=watches.email.thread#comment-625200>
>
Hello Daniele,
For the component of "fsl_debug_console" use the UART, so , in order to
analysis easily , i create one new project on ksdk1.3 about the frdm-kl46(kl46z256),
add the fsl_lpsci component , also configure it to UART0 , pay attention , i configure
the PTA1 PTA2 as the UART0 pins.Set two clock mode , FEI and PEE,
use the "clock configuration1"(PEE) mode as the
initialize mode , then change it to FEI.
In the main function , first send "abc", after change the clock mode , send "def", also can check the
current core clock : syt_test = CLOCK_SYS_GetCoreClockFreq();
Please test it on your side , maybe you need change the Pins of UART .
Hope it helps
Alice
Hello Alice,
sorry for the delay in the response but i had work on other project. Yes
you sample is working fine, i have change the clock crystal to 16Mhz and
use the fsl_debug instead the uart library. The problem born when you
select the clock source of the fsl_debug. If i select the autoselect
all work , but if i select
it crush. There is a bag ....
I use the ERCLK because i have a system that can go in low power
reducing the frequency, using the external clock (16Mhz) directly for
clock the system i can turn off the PLL and FLL.
Attached the sample with external cystal set to 16Mhz and the fsl_debug,
if you try the two setting in one case work, in the other not.
Thanks
--
*OPTOI GROUP *
Technical Dept.
Daniele Cortellazzi
***************************************************
OPTOELETTRONICA ITALIA S.r.l.
Via Vienna, 8
I-38121 Gardolo (TN) ITALY
Phone 0039 0461 991121
Fax 0039 0461 990164
daniele.cortellazzi@optoi.com
Hello Daniele,
The Clock cfg0 is FEI, so we can not use the ERCLK as the clock source
of UART0. In the CFG1 PEE mode , we can use it , so you can configure the
fsl_debug_console component as this :
And in the code , please add
Pay attention that , my project is from PEE mode to FEI mode , so when it change to FEI mode,
configure the UART clock source as "kClockLpsciSrcPllFllSel ".
Hope it helps
Alice
Hello,
attached there is the firmware. I'm using a kl46 with 16mhz crystal and
freertos. The function used are in:
- rtos_main_task.cwhere the init.c function is called and a
infinite loop print an "Hello"
- event.c where an interrupt PORTC_PORTD_IRQHandler call the
CPU_Clock_Setting function that change the frequency
Thanks
*
Il 07/03/2016 12:17, Alice_Yang ha scritto:
>
NXP Community
<https://community.freescale.com/?et=watches.email.thread>
>
fsl_debug problem change frequency
risposta da Alice_Yang
<https://community.freescale.com/people/Alice_Yang?et=watches.email.thread>
su /Kinetis Design Studio/ - Visualizza la discussione completa
<https://community.freescale.com/message/622056?et=watches.email.thread#comment-622056>
>
Hello,
yes with this sample it work. I have tried to disable the debug but same
proble happen with the TPM2 used like pwm. When i press a button the
function TPM_DRV_PwmStop(LCD_PWM_IDX, &LCD_PWM_ChnConfig0, 0); is called
and after that i switch the frequency:
if (CLOCK_SYS_GetCurrentConfiguration() != 1) {
error = CLOCK_SYS_UpdateConfiguration(1,
kClockManagerPolicyForcible);
//CLOCK_SYS_SetConfiguration(&clockMan1_InitConfig0);
i = CLOCK_SYS_GetCoreClockFreq();
//LPSCI_HAL_SetBaudRate(UART0_BASE_PTR, i, 115200);
I2C0_SetClockConfiguration();
ADC_SetClockConfiguration();
}
when the button is newely pressed i do
if(CLOCK_SYS_GetCurrentConfiguration() != 0){
error = CLOCK_SYS_UpdateConfiguration(0,
kClockManagerPolicyForcible);
//CLOCK_SYS_SetConfiguration(&clockMan1_InitConfig0);
i = CLOCK_SYS_GetCoreClockFreq();
//LPSCI_HAL_SetBaudRate(UART0_BASE_PTR, i, 115200);
TPM_DRV_SetClock(LCD_PWM_IDX, kTpmClockSourceModuleClk,
kTpmDividedBy32);
I2C0_SetClockConfiguration();
ADC_SetClockConfiguration();
}
to restore the cpu to higher frequency but when i call the function
TPM_DRV_PwmStart(LCD_PWM_IDX, &LCD_PWM_ChnConfig0, 0); it don't run
correctly. The MOD register is set to FFFFF bacause the function
CLOCK_SYS_GetPllFllClockFreq(); (called as in the image) return 0
Il 02/03/2016 10:30, Alice_Yang ha scritto:
>
NXP Community
<https://community.freescale.com/?et=watches.email.thread>
>
fsl_debug problem change frequency
risposta da Alice_Yang
<https://community.freescale.com/people/Alice_Yang?et=watches.email.thread>
su /Kinetis Design Studio/ - Visualizza la discussione completa
<https://community.freescale.com/message/620493?et=watches.email.thread#620493>
>
Hello,
the software remain in the infinite loop and can't exit, so my firmware is locked there. As visible in the image i see that the SendDataPolling is called by the debug_putc() but i can't reconstruct all the way. I can't see where the debug_putc is called so to debug the code, for do this i have to increase the number of nested function visible in kds.
Thanks