I have created a library in one project, but I can't seem to link to it in another project which uses it.
I have done:
Properties --> C/C++ Build --> Settings --> Tool Settings --> Libraries -->
1) added name of library in the -I field, without .a extension or "lib" prefix
2) added libraries physical location in the -L field.
I am still getting "undefined reference" to functions which I have double checked are in fact in the library.
Am I missing a something?
--Mike
已解决! 转到解答。
Hmm I just noticed I'm using "ObjectList" ( a text file) as the input of .o files to use. I did this to get around the Windows command line limit (8192 chars). I just saw this morning on mcuoneclipse.com that there is a fix for that. I wonder if this could be causing it?
Hi Erich,
Yes, the library I'm building is a GUI from Segger, it should build fine with a C++ application. Each .h file in the GUI has:
#if defined(__cplusplus)
extern "C" { /* Make sure we have C-declarations in C++ programs */
#endif
Furthermore, I was already building the entire GUI as part of my C++ application. It compiled and linked fine, but it was too many files, so I decided to make the GUI a library and link to it.
 
					
				
		
 BlackNight
		
			BlackNight
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		If you run the 'nm' utility (Defining Variables at Absolute Addresses with gcc | MCU on Eclipse), do you see the proper symbols?
Erich
Erich, I downloaded the new make (and rm and echo) as instructed here:
Solving the 8192 Character Command Line Limit on Windows | MCU on Eclipse
Now, I can link. However, the linker complains that the library I'm using does not have VFP (vector floating point) register arguments, but that my application does. Apparently this prevents me from linking.
So, do you know where the setting is that allows me change my library to use VFP arguments as well?
Found the setting, it's
Properties --> C/C++ Build --> Settings --> Target Processor --> Float ABI.
I set it to "FP instructions (hard)" on both my project and the library, I can now link successfully. Life is good... for now :--)
Hi Erich, here is the complete linker command line, as well as the output. I clipped the output a bit, because it was very long, but it just repeats over and over "undefined reference"...
'Invoking: Cross ARM C++ Linker'
arm-none-eabi-g++ -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -g3 -T "C:/M2/Project_Settings/Linker_Files/ProcessorExpert.ld" -Xlinker --gc-sections -L"C:/M2/Project_Settings/Linker_Files" -L"C:\kds_workspace\Segger-GUI\Debug" -Wl,-Map,"M2.map" -nanolibc -o "M2.elf" @ObjectList
./Sources/Application/Menu/Screen_Callbacks.o:(.data._ZL7_apFont+0x0): undefined reference to `GUI_Font16B_1'
./Sources/Application/Menu/Screen_Callbacks.o:(.data._ZL7_apFont+0x4): undefined reference to `GUI_Font20B_1'
./Sources/Application/Menu/Screen_Callbacks.o:(.data._ZL7_apFont+0x8): undefined reference to `GUI_Font8x16x2x2'
./Sources/Application/Menu/Screen_Callbacks.o:(.data._ZL7_apFont+0xc): undefined reference to `GUI_Font8x10_ASCII'
./Sources/Application/Menu/Screen_Callbacks.o:(.data._ZL7_apFont+0x10): undefined reference to `GUI_FontD24x32'
./Sources/Application/Menu/Screen_Callbacks.o:(.data._ZL7_apFont+0x14): undefined reference to `GUI_Font20B_1'
./Sources/Application/Menu/Screen_Callbacks.o: In function `showTextField(long, int, unsigned long, unsigned long)':
C:\M2\Debug/../Sources/Application/Menu/Screen_Callbacks.cpp:143: undefined reference to `WM_GetDialogItem'
C:\M2\Debug/../Sources/Application/Menu/Screen_Callbacks.cpp:144: undefined reference to `TEXT_SetBkColor'
C:\M2\Debug/../Sources/Application/Menu/Screen_Callbacks.cpp:145: undefined reference to `TEXT_SetTextColor'
./Sources/Application/Menu/Screen_Callbacks.o: In function `cbBkWindowCallback(WM_MESSAGE*)':
C:\M2\Debug/../Sources/Application/Menu/Screen_Callbacks.cpp:267: undefined reference to `GUI_SetBkColor'
C:\M2\Debug/../Sources/Application/Menu/Screen_Callbacks.cpp:268: undefined reference to `GUI_Clear'
Hmm I just noticed I'm using "ObjectList" ( a text file) as the input of .o files to use. I did this to get around the Windows command line limit (8192 chars). I just saw this morning on mcuoneclipse.com that there is a fix for that. I wonder if this could be causing it?