can't import IAR workbench example project in KDS (IAR plugged in)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can't import IAR workbench example project in KDS (IAR plugged in)

1,271 次查看
bhupendraprajap
Contributor II

Hello there,

I am trying to import a cloned KW01 connectivity software example in Kinetis design studio with IAR plugged in as mentioned on URL https://mcuoneclipse.com/2013/11/03/tutorial-replacing-iar-ew-with-eclipse-ide/ 

   (I am using a 30 days trial IAR Embedded Workbench 7.5 ) 

  1.       tried with importing with both options i.e. “create links” checked and unchecked but it shows the following error while including the header file SSD_FTFx.h:
  2.       Fatal error[Pe1692] while opening the file Flashinit.c
  1.       The above error keeps coming in any Flash related file i.e. sometimes it comes with Flashinit.c or sometimes it transfers to some other file and Flashinit.c works fine, simply I can’t get it
  2. Please help me resolve this.
标签 (1)
0 项奖励
回复
2 回复数

1,079 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bhupendra,

Sorry I haven't use this method to porting project from IAR to KDS.

I recommend you on one hand you can ask the author Erich of the tutorial you mentioned ,

on other hand you can directly create a new project on KDS, then copy the application code

into it .

BR

Alice

1,079 次查看
bhupendraprajap
Contributor II

Hi, Alice :smileyhappy:

Thanks for your Suggestion I am going to ask Mr. Erich 

Thanks Again.

0 项奖励
回复