can't import IAR workbench example project in KDS (IAR plugged in)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can't import IAR workbench example project in KDS (IAR plugged in)

1,272件の閲覧回数
bhupendraprajap
Contributor II

Hello there,

I am trying to import a cloned KW01 connectivity software example in Kinetis design studio with IAR plugged in as mentioned on URL https://mcuoneclipse.com/2013/11/03/tutorial-replacing-iar-ew-with-eclipse-ide/ 

   (I am using a 30 days trial IAR Embedded Workbench 7.5 ) 

  1.       tried with importing with both options i.e. “create links” checked and unchecked but it shows the following error while including the header file SSD_FTFx.h:
  2.       Fatal error[Pe1692] while opening the file Flashinit.c
  1.       The above error keeps coming in any Flash related file i.e. sometimes it comes with Flashinit.c or sometimes it transfers to some other file and Flashinit.c works fine, simply I can’t get it
  2. Please help me resolve this.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,080件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bhupendra,

Sorry I haven't use this method to porting project from IAR to KDS.

I recommend you on one hand you can ask the author Erich of the tutorial you mentioned ,

on other hand you can directly create a new project on KDS, then copy the application code

into it .

BR

Alice

1,080件の閲覧回数
bhupendraprajap
Contributor II

Hi, Alice :smileyhappy:

Thanks for your Suggestion I am going to ask Mr. Erich 

Thanks Again.

0 件の賞賛
返信