Hi there,
I am currently developing a little program to toggle GPIO pins. I am using KDS 3.0 and KSDK 1.2 with the TWR-K53N512 board. I am quite new in working with Freescale's MCUs. To toggle a GPIO pin is no problem but to time it with an interrupt is more complex. I want to use the LPTMR0 for this purpose.
My colleague gave me some code he used with another Freescale MCU and CW. Here is the part that makes problems:
static void IRQ_enable(uint32_t irq)
{
uint32_t div;
// Enable IRQ in NVIC
div = irq / 32u;
switch(div)
{
case 0u:
NVIC_ICPR0 |= 1 << (irq % 32u);
NVIC_ISER0 |= 1 << (irq % 32u);
break;
case 1u:
NVIC_ICPR1 |= 1 << (irq % 32u);
NVIC_ISER1 |= 1 << (irq % 32u);
break;
case 2u:
NVIC_ICPR2 |= 1 << (irq % 32u);
NVIC_ISER2 |= 1 << (irq % 32u);
break;
}
}
The problem is I do not find the NVIC registers. I know they are there according to the ARM website but they are not in the MK53D10.h file and there is no sysinit.h. The compiler, of coarse, says NVIC_ISER0 etc. are not declared. Anyone can help me? I guess its a simple solution. Thanks in advance!
Regards,
Kevin
已解决! 转到解答。
in KDS, NVIC related core registers are defined in core_cm4.h.
by default, it is under project\SDK\platform\CMSIS\Include
can you please take a look at it?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Nested Vectored Interrupt Controller( NVIC) is ARM register.
you can find the definition in attached document. search the doc with keyword "NVIC" you will know.
if you use KDS3.0, you can also view NVIC in debugger:
can this help?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi
1. are you sure your KDS version is 3.0. please check
is your side the same as below?
please make sure you use the latest version
Kinetis Design Studio Integrated Development |Freescale
2. did you do the same setting as below?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
In Eclipse, use the menu Help > Install New Software and use the following update site:
http://embsysregview.sourceforge.net/update
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Everything is the same except I have a newer Version of embsys (0.2.5). And that is not the problem.
The problem is not that I cannot see it in embsys but its missing in my header files (MK53D10.h etc.). They dont exist. Neither NCIVISER2 nor NVIC_ISER2 are declared, you know?
Maybe I have manipulated files but they are from KSDK...
Thanks for all your help.
Kevin
in KDS, NVIC related core registers are defined in core_cm4.h.
by default, it is under project\SDK\platform\CMSIS\Include
can you please take a look at it?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------