What is internal flash ram on mk20dx256vll10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is internal flash ram on mk20dx256vll10

846 Views
yarannan
Contributor III

Hi,

As question above, what is internal flash ram range on mk20dx256vll10. I didnt find on datasheet.

I've been trying all addresses on memory map, but Processor expert just doesnt like it. By the way,

I am trying to figure out a way to make an usb bootloader on KDS with processor expert.

 

Thanks,

 

Yaran

Labels (1)
0 Kudos
Reply
1 Reply

750 Views
DavidS
NXP Employee
NXP Employee

Hi Yaran,

Please look at the chip/device Reference Manual:

http://cache.freescale.com/files/32bit/doc/data_sheet/K20P100M100SF2V2.pdf 

Chapter 3.5.1.2 Flash Memory Sizes

FlexRAM address range is 0x1400_0000 - 0x1400_0FFF.

It can be used as generic RAM when not used as part of the FlexNVM functionality (aka EEPROM window).

Regards,

David 

0 Kudos
Reply