Use MIMXRT1052CVL5B Drive FT6336U

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use MIMXRT1052CVL5B Drive FT6336U

1,494件の閲覧回数
490538597
Contributor II

Use the SDK_2.5.0_MIMXRT1052xxxxB2\boards\evkbimxrt1050\emwin_examples\emwin_gui_demo drive the FT6336U TFT LCD. First I used the demo touchpanel code fsl_ft5406_rt.c, change the I2C_slave_ADDRESS,find the code run into the touch_event != kTouch_Reserved, PLEASE give me some advices. Thank you!

0 件の賞賛
返信
1 返信

1,268件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check my reply at below thread, Thanks.

https://community.nxp.com/thread/500945 


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信