Use K70 with MQX and PEG but with basic CW license. Which solution?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use K70 with MQX and PEG but with basic CW license. Which solution?

1,211 Views
arthurdeniau
Contributor I

Hi,

 

My project is to drive a TFT screen 65K colors, 800x480.

 

My environment it is following:

 

- Kinetis K70 (120)

- RTOS Freescale MQX 4.0.0

- PEG lite to have an easy GUI (Generate Cpp file, not Ainsi C, this is the source of my problem!)

- Codewarrior (v10.3) with a basic License perpetual (Available only for Ainsi C code, not C++)

 

So, all was ok until I tried to compile my project in CW with my Basic License. It does not accept C++ code (generated by PEG Windows Builder)

 

One solution is to buy Professional License. But the cost is too much.

 

Freescale propose to me use KDS. But I have some problem with my MQX version 4.0.0. I can't integrate it in KDS. I tried to convert my CW project, but wizard still blank (No windows appears to start project conversion)

 

It seem to me MQX 4.1 allows to devellop under KDS, but I also seen this MQX Beta version does not run on K70.

 

So what solution can I have to reach my objective? (K70 + RTOS MQX vx? + PEG (C++) + CW(basic license) / KDS? ...)

 

Thank for your feedback

Labels (1)
Tags (4)
0 Kudos
Reply
2 Replies

984 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Arthur Deniau,

it's not possible to work C++ with basic version CW.

i recommend you read this doc to see if this can help you on this problem:

https://community.freescale.com/docs/DOC-102594


it includes how to port CW10.6 MQX  project to KDS.



Best Regards,

Jennie

=================================================

this answer is for you. if it helps, please click on "Correct answer" button. thanks!



0 Kudos
Reply

984 Views
arthurdeniau
Contributor I

Hi,

Then I try to create a simple project:

- PEG windows builder: just 2 windows created, project is generated (*.cpp and .hpp are correctly generated)

Now, I just try to compile this under KDS with MQX 4.1.

Are they a simple way to create a new KDS project using MQX and then link our own SIMPLE application (created by Windows bulder. This simple application is just a static screen)?

0 Kudos
Reply