Unnecessary KDS PE project files under revision control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unnecessary KDS PE project files under revision control

828 Views
ky3orr
Contributor II

Hello All,

 

I am creating a project which will be available as an open-source.

I'd like to share it and do updates through one of available revision control systems like git, svn or p4.

 

I've noticed that every time I compile new software build some files are changing, even such I've not touched.

 

What are the files I shouldn't keep under revision control because KDS will generate them anyway from sources during compilation?

I am using KDS 2.0.0 + PE

 

Thanks for comments.

Best regards

 

Greg

Labels (1)
0 Kudos
Reply
1 Reply

625 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Grzegorz Kaczmarek,

This is discussed in the next thread in community:

KDS and Version Control


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply