Unnecessary KDS PE project files under revision control

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unnecessary KDS PE project files under revision control

814 次查看
ky3orr
Contributor II

Hello All,

 

I am creating a project which will be available as an open-source.

I'd like to share it and do updates through one of available revision control systems like git, svn or p4.

 

I've noticed that every time I compile new software build some files are changing, even such I've not touched.

 

What are the files I shouldn't keep under revision control because KDS will generate them anyway from sources during compilation?

I am using KDS 2.0.0 + PE

 

Thanks for comments.

Best regards

 

Greg

标签 (1)
0 项奖励
回复
1 回复

611 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Grzegorz Kaczmarek,

This is discussed in the next thread in community:

KDS and Version Control


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复