Unable to Debug after KDS Update

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to Debug after KDS Update

4,105 次查看
nikolaykulikov
Contributor I

After a fresh install of KDS3.0.0, everything works. Once I do a software update I can no longer debug.

I have tried starting a new work space and that doesn't help.

 

Installed software of my KDS:

  Component Development Environment    1.8.0.RT7_b1515-1052

  Component Development Environment Documentation    1.1.0.RT7_b1515-1052

  Documentation for Kinetis Design Studio V3.0.0    4.0.0

  Embedded Systems Register View (SFR)    0.2.4.r178

  FSL Eclipse Updater Custom Actions Feature for Eclipse 4.4.x    2.0.12.FSL_150303

  GNU ARM C/C++ Cross Compiler    1.14.1.201508011813

  GNU ARM C/C++ J-Link Debugging    3.2.1.201508011813

  GNU ARM C/C++ OpenOCD Debugging    3.2.1.201508011813

  GNU ARM PEMicro Interface Debugging Support    2.1.5.201507151627

  Kinetis Design Studio    3.0.0

  KSDK 1.2.0 Eclipse Update    1.0.1.b150603

  MQX RTOS Project of Projects    1.1.8.201504151538

  MQX RTOS Task Aware Debugger for GDB    1.0.8.201504151538

  Processor Expert for Kinetis    3.0.0.RT7_b1515-0427

  Processor Expert for Kinetis 3.0 - Patch 1    1.0.0.b150505

  Project of Projects    1.1.8.201504141312

 

After trying to start debugging error message, stated on the screenshot.

Discussion inUnable to Debug after KDS Update It did not help.

标签 (1)
0 项奖励
回复
7 回复数

3,655 次查看
BlackNight
NXP Employee
NXP Employee

I can reproduce that problem on my machine: using the latest GNU ARM Eclipse plugins causes J-Link and QUEMU to fail. I have filed a bug ticket on SourceForge and contacted the maintainer directly.

https://sourceforge.net/p/gnuarmeclipse/bugs/192/

Erich

0 项奖励
回复

3,655 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Nikolay Kulikov,

thank you for good description of the issue. Please, what do you use for the system? Do you have Linux distribution 64-bit?

Actually I compare it with my updates in Installed Software and I don´t see something wrong.

So, I´m going to try it in Ubuntu 14.04.2 and tell you more.

Thank you for your feedback!

Iva

0 项奖励
回复

3,655 次查看
nikolaykulikov
Contributor I

Yes, I use a 64-bit Linux.

In Windows XP, these same problem:Screenshot - 08042015 - 12_01_23 PM.png

0 项奖励
回复

3,655 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Nikolay,

It is strange,

please, do you have correctly set debugger?

debug2.png

What do you use for interface?

Do you have the newest firmware for your interface?

Regards!,

Iva

0 项奖励
回复

3,655 次查看
nikolaykulikov
Contributor I

Hello, Iva!

I use FTDI interface on FT2232 debugger. Firmware of debugger correctly and working.

I use a bunch Openocd-GDB for debugging other families mikrokontrollers in KDS3.0.0 - there is no problem. Problem arise when i use Kinetis microcontrollers.

This is a topic where the problem went: https://community.freescale.com/message/535933#535933

When installing without updates KDS3.0.0 under GDB debug server is not running. After updating the KDS - do not run the appropriate plug-in Eclipse. The screenshots setting Openocd session under Linux and Windows.

lin.pngwin.png

0 项奖励
回复

3,655 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Nikolay,

thank you for your feedback, more customers face this issue, currently we work on the solution.

It is the same issue as Unable to Debug after KDS Update​ with J-Link.

I will let you know.

Best Regards,

Iva

0 项奖励
回复

3,655 次查看
nikolaykulikov
Contributor I

I use PE Multilink in other projects in the Kinetis K60. With this debug interface operating is normally.

On this particular board is not possible to connect to anything other than FT2232, so i use Openocd.

0 项奖励
回复