USBDM Updated for KDS 3.0.0 and KSDK 1.2.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USBDM Updated for KDS 3.0.0 and KSDK 1.2.0

1,467 次查看
pgo
Senior Contributor V

Dear All,

 

USBDM has been updated to support the latest versions of KDS and KSDK.

 

A video introduction is available at:

USBDM with Kinetis Design Studio and Kinetis SDK - YouTube

 

The software is available at:

USBDM | SourceForge.net

 

More information is available at:

USBDM: USBDM Debugger interface for Freescale RS08,HCS08,HCS12,Coldfire and ARM-Kinetis Devices.

 

  • USBDM is a debugger hardware interface for a range of Freescale micro-controllers. It is designed to work with Freescale's Codewarrior software under Windows and Linux.
  • It also provides support for Coldfire with the M68K GNU Tool chain or Kinetis with ARM Ltd GNU Tools for ARM.
  • A set of stand-alone programmers for HCS08, HCS12, Kinetis and Coldfire are also provided.

 

Enjoy.

标签 (1)
0 项奖励
回复
2 回复数

1,071 次查看
carlos_cuevas
Contributor I

Hi PGO, the latest windows installer (v4.12.1.80) doesn't support installing the dlls into FreeMaster, I tried copying them manually but I can't get them to work, is there something I can do to use USBDM with FreeMaster? Do you plan to add support for FreeMaster in the future or it's a deprecated feature? Thanks!

0 项奖励
回复

1,071 次查看
pratiekbhadrana
Contributor III

This is even better than the original solution of using USBDM with KDS. Thanks pgo.

0 项奖励
回复