The default link file for Kv10 NPW project is not correct

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The default link file for Kv10 NPW project is not correct

Jump to solution
2,396 Views
jack
Contributor III

hello,

 

I have started to use KDS beta v1.0.1. Here is a minor issue may need to be fixed: Creating a new kv10 project using wizard (without PEx), but the link file is actually for kl25.

 

I also noticed that "Parallel build" is not enabled by default for a new created project. It will take much longer time to build a project without enabling "Parallel build". I think this option should be enabled by default, right?

 

Jack

Labels (1)
0 Kudos
Reply
1 Solution
2,273 Views
BlackNight
NXP Employee
NXP Employee

Hi Jack,

yes, that problem with the 'bare' projects creating KL25z linker files is noted in the release notes (Kinetis Design Studio V1.0.1 Beta Release Notes) under 3) Known Issues, Project Creation, Issue 1.

About "Parallel Build": yes, this has been noted as something we want to improve for the V1.1 GA release after beta.

Thanks for your feedback!

Erich

View solution in original post

0 Kudos
Reply
1 Reply
2,274 Views
BlackNight
NXP Employee
NXP Employee

Hi Jack,

yes, that problem with the 'bare' projects creating KL25z linker files is noted in the release notes (Kinetis Design Studio V1.0.1 Beta Release Notes) under 3) Known Issues, Project Creation, Issue 1.

About "Parallel Build": yes, this has been noted as something we want to improve for the V1.1 GA release after beta.

Thanks for your feedback!

Erich

0 Kudos
Reply