The default link file for Kv10 NPW project is not correct

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The default link file for Kv10 NPW project is not correct

ソリューションへジャンプ
2,461件の閲覧回数
jack
Contributor III

hello,

 

I have started to use KDS beta v1.0.1. Here is a minor issue may need to be fixed: Creating a new kv10 project using wizard (without PEx), but the link file is actually for kl25.

 

I also noticed that "Parallel build" is not enabled by default for a new created project. It will take much longer time to build a project without enabling "Parallel build". I think this option should be enabled by default, right?

 

Jack

ラベル(1)
0 件の賞賛
返信
1 解決策
2,338件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jack,

yes, that problem with the 'bare' projects creating KL25z linker files is noted in the release notes (Kinetis Design Studio V1.0.1 Beta Release Notes) under 3) Known Issues, Project Creation, Issue 1.

About "Parallel Build": yes, this has been noted as something we want to improve for the V1.1 GA release after beta.

Thanks for your feedback!

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,339件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jack,

yes, that problem with the 'bare' projects creating KL25z linker files is noted in the release notes (Kinetis Design Studio V1.0.1 Beta Release Notes) under 3) Known Issues, Project Creation, Issue 1.

About "Parallel Build": yes, this has been noted as something we want to improve for the V1.1 GA release after beta.

Thanks for your feedback!

Erich

0 件の賞賛
返信