The FRDM-K66F device is not showing in KDS 3.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The FRDM-K66F device is not showing in KDS 3.2

Jump to solution
1,745 Views
sivaveluppillai
Contributor III

The FRDM-K66F device is not showing in KDS 3.2  

I remember the getting started link for the FRDM-K66F did have a special SDK 1.3 for the board FRDM-K66F but now this is missing.

http://www.nxp.com/products/software-and-tools/hardware-development-tools/freedom-development-boards...

 

The FRDM-K66F may be removed for some reason?

I have installed the special SDK onto one of the PC as a copy but the project generator not picking of this folder.

Any idea what is going on?

Labels (1)
0 Kudos
Reply
1 Solution
1,591 Views
sivaveluppillai
Contributor III

My issue was the device FRDM-K66 was not showing in the device list.

File => New => Kinetis SDK1.x Project (Next) Devices => Boards => Kinetis

 

I still haven’t found a solution for this issue!

 

But it seems the SDK SDK_2.0_FRDM-K66F is the best way for loading samples as I can compile and run the sample code without any issue.

Thanks

View solution in original post

0 Kudos
Reply
3 Replies
1,591 Views
sivaveluppillai
Contributor III

All resolved using SDK2.

0 Kudos
Reply
1,591 Views
MarekTrmac
NXP Employee
NXP Employee

Hi Siva,

go to http://kex.nxp.com and create configuration for FRDM-K66F. You can download SDK 2.0 (latest version).

Regards

Marek

1,592 Views
sivaveluppillai
Contributor III

My issue was the device FRDM-K66 was not showing in the device list.

File => New => Kinetis SDK1.x Project (Next) Devices => Boards => Kinetis

 

I still haven’t found a solution for this issue!

 

But it seems the SDK SDK_2.0_FRDM-K66F is the best way for loading samples as I can compile and run the sample code without any issue.

Thanks

0 Kudos
Reply