TWR-K70 OSC0 Setting in KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K70 OSC0 Setting in KDS

Jump to solution
770 Views
waqasbutt
Contributor II

On TWR-K70 OSC0 is 50MHz. I can't set it in KDS. Any ideas?

 

174849_174849.pngPicture 2017-01-20 09_38_46.png

Labels (1)
0 Kudos
Reply
1 Solution
658 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Waqas Butt,

You select clock source as "crystal", however the maximal crystal value is 32Mhz.

you need select clock source as "External reference clock" which allows to set 50MHz clock frequency .

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
659 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Waqas Butt,

You select clock source as "crystal", however the maximal crystal value is 32Mhz.

you need select clock source as "External reference clock" which allows to set 50MHz clock frequency .

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply