Hello guys!
I've a problem with TSS_Library when I try validate the example following: http://cache.freescale.com/files/videos/player/TIP_popupvideo.html?XML=/files/videos/training/genera...
That example use the TSS Library that control brightness of the LED with sensor touch.
Two unexpected behaviors occur when I try to use TSS Version 3.0 or 3.1.
TSS Version - TSS_3_0:
fatal error: TSS_SensorTSIL_def.h: No such file or directory
TSS Version - TSS_3_1:
undefined reference to `TSS_SetSystemConfig'
Details:
* I'm using the KDS at version 3.0.1.
* I'm using Processor Expert for build the code.
* I'm using FRDM-KL25Z
Anybody can help me!
Thanks
已解决! 转到解答。
Hello Arnaldo,
The "ASLIDER" control Type only can used on TSS_3.0 ,
and on the KDS v3.0, it seems have a bug on use the TSS_3.0 .
Please use the KDSv3.2 , you can download and install refer to here : New Kinetis Design Studio v3.2.0 available
Hope it helps
Hello Alice!
After your tips I had the following behaviour don't work to TSS_3_0. However when I chosse library TSS_3_1 and Control Type equal the ASLIDER I have other erro message (see figure bellow).
It's possible you validate the example "http://cache.freescale.com/files/videos/player/TIP_popupvideo.html?XML=/files/videos/training/genera..." using the Kinetis Desing Studio?
Thanks!
Regards,
Arnaldo
Hello Arnaldo,
The "ASLIDER" control Type only can used on TSS_3.0 ,
and on the KDS v3.0, it seems have a bug on use the TSS_3.0 .
Please use the KDSv3.2 , you can download and install refer to here : New Kinetis Design Studio v3.2.0 available
Hope it helps
Hello Arnaldo,
Does this thread can help you ? Start working with NXP Touch Software library
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Alice!
First all I'd like say thank you for your time :-)
I tested the link (Start working with NXP Touch Software library) and worked perfect.
But I think my problems keep on... I'll try explain you... If Freescale provide TSS library, that occasion it worked at codewarrior, I guess the library should work too Kinetis Design Studio, don't you? Probably, the library should work KDS, but I don't understand how!
For example: in "TSS Version - TSS_3_0:
fatal error: TSS_SensorTSIL_def.h: No such file or directory" realy the file TSS_SensorTSIL_def.h doesn't exist inside the folder TSS (see the figure bellow).
The big question for me at this moment is: there is some kind configuration in KDS for to work with TSS Library?
Have a nice day,
Arnaldo
Hello Arnaldo,
I know your meaning, you want use the TSS_Library of PE driver on KDS.
Yes, it can used , while after you add the TSS component , you need configure two place:
Please refer to below steps to configure :
Then build the project, the error will disappeared .
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Alice,
I'm having the same problem described in the beginning of this thread.
I've already made the linker see the TSS_KXX_M0 library. The error persists. Looks like the only thing happening is that really there isn't the TSS_SensorTSIL_def.h file. When I double click to open the file in the Project Explorer window, under my project folder, Sources>TSS>TSS_SensorTSIL.c, it simply doesn't. The only thing it does is to show the incude Processor Expert generate in the TSS_SensorTSIL.c file.
I don't think I will be able to make it work, neither anybody else, without this file.
I can't see any other reason why it doesn't work or the compiler doesn't find it.
Hopping to hear from you.
Vítor Pereira