TSS_Library doesn't build

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TSS_Library doesn't build

跳至解决方案
4,487 次查看
arnaldogomes
Contributor III

Hello guys!

 

I've a problem with TSS_Library when I try validate the example following: http://cache.freescale.com/files/videos/player/TIP_popupvideo.html?XML=/files/videos/training/genera...

That example use the TSS Library that control brightness of the LED  with sensor touch.

 

Two unexpected behaviors occur when I try to use TSS Version 3.0 or 3.1.

TSS Version - TSS_3_0:

fatal error: TSS_SensorTSIL_def.h: No such file or directory

 

TSS Version - TSS_3_1:

undefined reference to `TSS_SetSystemConfig'

 

Details:

* I'm using the KDS at version 3.0.1.

* I'm using Processor Expert for build the code.

* I'm using FRDM-KL25Z

 

Anybody can help me!


Thanks

标签 (1)
标记 (1)
1 解答
3,978 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Arnaldo,

The "ASLIDER" control Type only can used on TSS_3.0 ,

and on the KDS v3.0, it seems have a bug on use the TSS_3.0 .

Please use the KDSv3.2 , you can download and install refer to here : New Kinetis Design Studio v3.2.0 available

pastedImage_1.png

Hope it helps

在原帖中查看解决方案

0 项奖励
回复
9 回复数
3,978 次查看
arnaldogomes
Contributor III

Hi Alice!

Know works!

Thanks!

Regards,

Arnaldo

0 项奖励
回复
3,978 次查看
arnaldogomes
Contributor III

Hello Alice!

After your tips I had the following behaviour don't work to TSS_3_0. However when I chosse library TSS_3_1 and Control Type equal the ASLIDER I have other erro message (see figure bellow).

pastedImage_1.png

It's possible you validate the example "http://cache.freescale.com/files/videos/player/TIP_popupvideo.html?XML=/files/videos/training/genera..." using the Kinetis Desing Studio?

Thanks!

Regards,

Arnaldo

0 项奖励
回复
3,979 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Arnaldo,

The "ASLIDER" control Type only can used on TSS_3.0 ,

and on the KDS v3.0, it seems have a bug on use the TSS_3.0 .

Please use the KDSv3.2 , you can download and install refer to here : New Kinetis Design Studio v3.2.0 available

pastedImage_1.png

Hope it helps

0 项奖励
回复
3,978 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Arnaldo,

Does this thread can help you ? Start working with NXP Touch Software library

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,978 次查看
arnaldogomes
Contributor III

Hello Alice!

First all I'd like say thank you for your time :-)

I tested the link (Start working with NXP Touch Software library) and worked perfect.

But I think my problems keep on... I'll try explain you... If Freescale provide TSS library, that occasion it worked at codewarrior, I guess  the library should work too Kinetis Design Studio, don't you? Probably, the library should work KDS, but I don't understand how!

For example: in "TSS Version - TSS_3_0:

fatal error: TSS_SensorTSIL_def.h: No such file or directory" realy the file TSS_SensorTSIL_def.h doesn't exist inside the folder TSS (see the figure bellow).

pastedImage_5.png

The big question for me at this moment is: there is some kind configuration in KDS for to work with TSS Library?

Have a nice day,

Arnaldo

0 项奖励
回复
3,978 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Arnaldo,

I know your meaning, you want use the TSS_Library of PE driver on KDS.

Yes, it can used , while after you add the TSS component , you need configure two place:

  1. Add the TSS library to the linker options
  2. Change compiler option to accept asm("...")

Please refer to below steps to configure :

pastedImage_0.png

pastedImage_1.png

Then build the project, the error will disappeared .

Hope it helps
Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,978 次查看
vítorpereira
Contributor III

Hi Alice,

I'm having the same problem described in the beginning of this thread.

I've already made the linker see the TSS_KXX_M0 library. The error persists. Looks like the only thing happening is that really there isn't the TSS_SensorTSIL_def.h file. When I double click to open the file in the Project Explorer window, under my project folder, Sources>TSS>TSS_SensorTSIL.c, it simply doesn't. The only thing it does is to show the incude Processor Expert generate in the TSS_SensorTSIL.c file.

pastedImage_5.png

I don't think I will be able to make it work, neither anybody else, without this file.

I can't see any other reason why it doesn't work or the compiler doesn't find it.

Hopping to hear from you.

Vítor Pereira

3,978 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Vitor,

Which version of KDS do you used ? Please use the latest version of KDS v3.2.0

Hope it helps

Alice

0 项奖励
回复
3,978 次查看
vítorpereira
Contributor III

Hi Alice,

I am using the latest version of KDS, the KDS v3.2.0.

Vítor Pereira

0 项奖励
回复