Sensor fusion using KDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sensor fusion using KDS

1,011 次查看
moelf
Contributor I

Hi,

 

I tried to run freescale sensor fusion using KDS, and I get the following error:

Launching 'FSFK_kl25z.elf' has encountered a problem  Error starting process

 

Any help will be appreciated.

 

Thanks.

 

Best.

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

875 次查看
BlackNight
NXP Employee
NXP Employee

Hi Mo,

good timing, as I'm exploring the sensor fusions projects myself right now too, for my quadrocopter project (Kinetis Drone: Driving the Electronic Speed Controllers​). What I realize and see is that the debug configurations in these sensor fusion projects are not properly configured. It looks the projects have been renamed without updating the debug configurations.

Erich

0 项奖励
回复

875 次查看
BlackNight
NXP Employee
NXP Employee

Hi Mo,

digging into it, I have found unfortunately several issues in the project setup.

Good news is: I have the SensorFusion5\KDS\KDS3 FRDM 3DOF Bare Board Tiltmeter\FRDM_KL25Z project running sucessfully now (attached).

Bad news is: I'm able to build and debug the SensorFusion5\KDS\KDS3 FSFK\FSDK_KL25Z too, but it fails at runtime as this demo expects the MultiB shield.

It seems not be prepared and working just with the accelerometer on the board.

I have that project attached for you too.

Just in case this helps,

Erich

0 项奖励
回复