Re: DAC not working on FRDM-K22F ver 2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: DAC not working on FRDM-K22F ver 2

1,110 Views
julioruzicki
Contributor II

HI guys, I'm also having troubles to make the DAC works. I tried your previuos tips but unsuccessfully. I'm using kinetisstudio 3.0.2 and k22f.

Could you help me?

Labels (1)
3 Replies

999 Views
DavidS
NXP Employee
NXP Employee

Hi Julio,

I dug up the old example I had and configured it to do simple ramping of DAC0_OUT to J24 pin 11 of FRDM-K22F using the KDS3.0.2+PE.

Hope it helps.

Regards,

David

999 Views
julioruzicki
Contributor II

Hi David, thanks by your attention. Your code is working but I don't know why, because is similar like examples.

I'll install de version 3.2.0 linux and verify. Some weeks ago I had a similar problem with USB stack but I could solve.

Thank you again.

0 Kudos
Reply

999 Views
DavidS
NXP Employee
NXP Employee

Hi Julio,

Glad to help.

If question answered please mark it correct.

Regards,

David

0 Kudos
Reply